This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC输出功率的估计

Other Parts Discussed in Thread: DAC3484

请问DAC的输出功率如何估计?比如DAC3484。谢谢!

  • Hi Yi qin,

    DAC的输出功率与DAC的类型(电流型还是电压型)以及外围电路阻抗大小有关。

    如DAC3484为电流型DAC,单端输出电流为0~20mA,DC电流为10mA,在指标书中1:1balun的连接方式情况下,单端面对的阻抗为(50||50)||25=12.5欧姆,因此单端的电压峰峰值为20mA*12.5欧姆=0.25Vpp,则差分电压峰峰值为0.5Vpp。最后根据电压峰峰值及阻抗大小算出输出功率。

  • 输出功率和很多因素有关,输入数据,输出电流,内部NCO增益,Gain的增益,offet的增益,DAC和调制器之间的滤波器损耗等。

  • 推荐你看一下这篇文档吧

    中文的

    http://www.ti.com.cn/cn/lit/an/zhca119/zhca119.pdf

    专门介绍3484输出功率计算的

  • 如果以单音信号为标准,输出匹配是按照评估板原理图设计,那么最大输出功率就是略微低于+7dBm(不开QMC的前提下)。

    如果打开QMC,并将增益设为适当的中间值1447,那么最大输出功率则略微低于+4dBm。

    其它调制信号,请根据峰均比进行功率回退。