Dear TI engineer,
I have been using LAUNCHXL_F28379D to communicate with DAC71408 and have been having communication problems. May I ask whether the two SPI signals are at the same level? Do I need to add a level switching chip to the circuit?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI engineer,
I have been using LAUNCHXL_F28379D to communicate with DAC71408 and have been having communication problems. May I ask whether the two SPI signals are at the same level? Do I need to add a level switching chip to the circuit?
您好,
DAC71408的SPI电平标准是VIO电压,您使用的VIO电压是多少?
您可以看下 LAUNCHXL_F28379D的SPI电平是多少?或者实际测量下其输出的高电平电压看是多少?
LAUNCHXL_F28379D的SPI电平需与DAC71408的SPI电平相兼容,否则的话不能正常通信。
Yes, they can communicate with each other properly if they are all 3.3V. If communication does not work properly, it should be a problem elsewhere