This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8831IBD遇到问题



尊敬的TI技术专家:

   这是我第一次用可以接运放输出双极性电压的16位DA。我发上了我电路图,是按照datasheet里双极性的接法。刚开始用输出值与我的程序给定值是一样的 可是过段时间后DA输出值就与我程序的给定值不一样了。然后我换一个DA就好了,可是又过不到几天又出现同样问题。接连换了4块DA,都是这样。关键的这四片DA的错误输出值都是一样的。比如我程序给0.3V,输出都为1.26V ,程序给1V,输出都为1.09V.觉得这个现象很奇怪 我现在也不敢再拿新的DA尝试了 不知道DA到底有没有坏 如果坏了 为什么都输出同样的错误值呢??

 这是单电源供电的,5V的电源给的很准,还有手基本没怎么摸芯片,静电的情况也可以排除。希望能够帮我解答下!谢谢!