Part Number: ADS6142
Other Parts Discussed in Thread: THS4509
非常感谢,请问下如果我使用图98的设计,该如何选取RS,RT,RG,RF的阻值呢?他们是否有一个选取范围来使得芯片发挥更好的作用。还有Rfil和Cfil,是否有一个参考范围?还是任意选取只有满足自己所需的低通滤波截止频率就可以呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,Figure 98的THS4509的反馈电阻Rf和增益电压Rg的取值可以参考THS4509的数据手册,反馈电阻选择的是348ohm,根据不同的增益得到不同的Rg。另外输入阻抗Rit的值在Table3中也有给出。 Figure98中的Rs//RT即为Rit。。

THS4509的输出和ADC的隔离电阻Rfil可选取50ohm终端匹配电阻,Cfil可根据低通滤波器的截止频率计算得到。