我正在使用ads1298做ecg应用,但是不太确定是使用单电源供电还是双电源供电。比如单电源方式给模拟部分供给3v,或者使用双电源方案供给+1.5v和-1.5v。
因此想咨询下两种供电方式的差别和优劣,
期待回复,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,ADS1298的模拟电压AVDD和数字电压DVDD都是单电源供电的,如下电气参数表格,AVDD的电压范围为2.7V~5.25V,数字电压的电压范围为1.65V~3.6V。
AVDD-DVDD的范围在-2.1V~3.6V。
您提到单电源和双电源的差异,基本上运放都是既能单电源又能双电源供电的,二者的主要差异就是双电源能够处理负压信号,比如输入信号有负半轴信号,而单电源只能处理正半轴的信号。 还有些比如需要处理0V~的信号,运放即使单电源供电,但是输入不能到电压轨,因此也就无法处理0V附近的信号, 也是建议采用双电源供电。
请问ecg采集使用单电源给ads1298提供模拟部分的供电可以吗?会采集不到信号吗
是的,ADS1298使用单电源供电。
信号要保证在ADS1298的输入共模电压范围内,也要保证差分输入VinP-VinN的电压范围,详细参考数据手册的9.3.1.5.1和9.3.1.5.2部分。
心电信号的幅值范围为多少?满足上面的输入电压范围就没问题。