目前,在自行设计ADS1299的采集装置,关于60,61,62,63引脚的连接不太明白。希望可以告知这几个引脚的功能以及连接方式。以下为连接方式,BIAS_IN 连接脑电帽上的电极
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
60,61,62,63这几个管脚其实是引出的 ADS1299内部集成的偏置运放的管脚,如下截图所示,

当为偏置运放选择了适当的通道、在芯片外部接上反馈元件形成闭环环路时,偏置信号在BIASOUT引脚处可用。该信号可以在滤波后输入,也可以直接输入BIASIN引脚,如上截图33所示。通过寄存器的MUX位设置为“110”(P侧)或“111”(N侧),可以将该BIASIN信号复用到任何输入电极。图33显示了从通道1、2和3生成并路由到通道8的N侧的偏置信号。此功能可用于动态更改电极,电极用作驱动患者身体的参考信号。
线路连接没问题,关于R8 和C26参数,它们决定了BIAS环路的带宽,用户可以根据特定应用更改这些值以设置带宽。
ADS1299EEG-FE 是EEG信号采集的应用,您可以查看下面用户指南 第7部分,了解更多EEG应用信息: