This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
供电电压实测是多少?
SPI主控端的电平是多少?是否与DAC80501电平兼容?主控端是否与DAC80501共地?
您可以附上原理图吗?我先看下原理图
很高兴您的SPI通信已经正常,感谢您的反馈~
DAC80501使用3.3V供电是没问题的,您是否实际测量了供电管脚的电压是3.3V?
VREFIO管脚您是否接了其他负载?内部基准电压输出电流能力是5mA,如果外接了其他负载,可能会拉低其基准电压的输出。
另外,也建议您附上原理图以做进一步检查。
您好,很抱歉我没有及时看到消息,我们的问题还没有解决但原理图暂时无法提供,供电管脚的电压是3.3V,VREFIO管脚接了10uf+0.1uf的电容,还给ADS1220提供基准
内部基准电压输出精度在1%,在2.4975V ~ 2.5025V之间,误差±25mV。如果输出2.39V,误差是比较大的了。
您测试了几块板子是这种情况?是否可以多测试几块板子以排除焊接问题?
也请您确认下DAC80501的物料来源,其最终进货渠道是否为TI?
为排除物料问题,您可以在TI官网申请或购买几片样片吗?以进行测试
在下面链接DAC80501产品主页,点击右上角“理解订购”,网页会自动滑到“订购和质量”版块,其中 DAC80501MDGSR可以申请样片,也可在左边合适的型号处输入“添加到购物车”的数量以进行购买。