This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC5672IPFBR的输入通道问题



我刚接触电路设计,很多不懂,希望得到大家的帮助!对于这个芯片,我设置的电压是3.3V。请问那对于14位的通道,如果每个数据都是“1”,那总的数据量是2的14次方,大概是2万个数据,那对于最低有效位,是不是它的电流是3.3/20000.差不多是150微伏呢?我不懂,希望专业人士告知。另外对于GSET,MODE,SLEEP 的设置,如果我已经选择了dual-bus模式,是不是MODE就可以直接接DVDD?