This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12J2700: Line Rate和输出数据格式

Part Number: ADC12J2700

你好。

我现在有两个问题:

配置条件:

Bypass Mode, No Decimation, DDR = 1, P54 = 0, LMF = 8,8,8。

DEVCLK+/-=2048MHz。FPGA是xilinx的xc7vx485tffg1158-2。

问题1:虽然手册说了BIT RATE=ADC CLOCK *2,即JESD204B的Line Rate=2.048*2=4.096Gbps,但是我还是不明白Line Rate是什么计算得到的?即详细的计算过程;

问题2:ADC12J2700在与xilinx的FPGA的JESD204B核相连后,FPGA端输出的数据格式是什么?因为我要解析出数据格式,以便下面的下变频用。

希望尽快得到答复。谢谢。