This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1278的参考电压问题



ELECTRICAL CHARACTERISTICS中提到,

Vrefn的输入范围是AGND-0.1 to AGND+0.1V,

而Vrefp与CLK有关,以0.1 < fCLK <27MHz为例,Vrefp输入范围为0.5到3.1V

而后文又提到,参考输入电压的范围为AGND-0.4v to AVDD+0.4v

问题1. 这个参考电压的要求到底是怎样的?

问题2. ELECTRICAL CHARACTERISTICS中还提到Common-mode input voltage是2.5v,这个是对输入信号的要求,还是只是文档列举的一个应用场景?

  • Hi yq,

       Vrefn可以认为是AGND,VREF=Vrefp-Vrefn,对你举的例子来说,Vrefp在0.5到3.1V,这些是正常工作的范围。

       AGND-0.4v to AVDD+0.4v的范围是ESD保护的要求,器件手册中有详细的描述。

  • hi nick, thanks for your reply

    假定vref为2.5v,那么能测量的信号在正负2.5之间,再考虑到2.5伏共模电压,模拟输入的幅度就是1.25~3.75之间,是这样吗?

    另外,若参考电压超3.1v,但未超avdd+0.4v,会发生什么?只是输出结果可能不正确,还是其它什么?