This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65MLVD082 issue

Other Parts Discussed in Thread: SN65MLVD082

Dear all,

使用SN65MLVD082中出现以下问题。急!!!!!!

由于端子走线和板卡的限制,是无法做到同时满足单端走线阻抗50,差分走线阻抗100;总线背板上考虑10块板卡的位置,间距25.4mm;我在每个M-LVDS驱动器的输出均串联了22欧姆电阻,背板上总线两端的匹配电阻若改用阻值如100、82的时候,示波器观察驱动板卡旁边的接收板卡上芯片(TYPE-II型)M-LVDS侧的信号(时钟信号,125MHz),上升沿裕度很小,甚至上升沿的振铃已经低于150mV,改用51欧姆电阻,虽然信号幅度下降,只有+/-250mV,上升沿裕度能保证在100mV以上。
       1、使用51欧姆电阻是否存在问题,是否会因为高低温环境变化导致驱动能力不足,引起幅度变化,造成通信出错,这个目前没有条件在高低温下测量。使用提供的ibis模型仿真,slow和fast模型对应高温85和低温-40,结果幅度没有变化,只是上升速率的变化,是否可信。
       2、驱动器接收一直使能,发送0,当发送使能关闭的时候(即输出差分从0变为高阻),会有一个过冲,幅度超过50mV,因此接收端自身会采集到一个脉冲,邻近板卡接收端信号没有问题。

能否给出参考建议解决这个问题?