This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【求助】

Other Parts Discussed in Thread: ADS1298

 

各位工程师好,现有一个关于ADS1298的问题,请看一下。

我采用的是ADS1298-PDK硬件设计,其中AVDD =  +2.5V ,  AVSS = -2.5V,原来设计的是 DVDD = 3.3V.现在我将DVDD更改为1.8V供电,其他不变.

请问一下,这样更改DVDD大小除了会影响SCLK的最大速率,还有无其他影响呢?

这样的设计,ADS1298能否正常工作?(我现在的ADS1298感觉一直没有正常工作)


Thanks in advance!

  • 数字接口的电平输入输出值的变化考虑了吗

    •  谢谢Carter Liu 
    • 我想问一下,“数字接口的电平输入输出值的变化” 指的是START和DRDY 的电平值吗? 我现在已经测到了这些端口的高电平值是1.8V,和DVDD一致。
    • 问题背景:我将DSP和ADS1298相连接,因为DSP的高电平值为1.8V,故我想采用不使用电平转换芯片的方案,也即让ADS1298数字信号产生的高电平值都为1.8V,让两者进行通信和控制。现在将DVDD改为1.8V供电后,出现DRDY 返回信号不正常,如下图(信号线2)所示,DRDY返回信号是一直低电平,偶尔返回高电平信号。
    • 请再详细解释一下吧!非常感谢!