手册上说CDCLVD2102前端输入可以为2.5V LVCMOS电平,可我前端时钟输入为3.3V LVCMOS电平,手册上要求进行输入摆幅控制,并且要求3.3 V LVCMOS clock input swing needs to be limited to VIH≤VCC。请问我可以通过分压的方式实现吗,输入时钟信号为60MHz。这样分压处理会不会引起时钟波形失真或者抖动?如果不可以,怎么将3.3V LVCMOS转换成2.5V LVCMOS处理会比较好?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
手册上说CDCLVD2102前端输入可以为2.5V LVCMOS电平,可我前端时钟输入为3.3V LVCMOS电平,手册上要求进行输入摆幅控制,并且要求3.3 V LVCMOS clock input swing needs to be limited to VIH≤VCC。请问我可以通过分压的方式实现吗,输入时钟信号为60MHz。这样分压处理会不会引起时钟波形失真或者抖动?如果不可以,怎么将3.3V LVCMOS转换成2.5V LVCMOS处理会比较好?谢谢!
是的,CDCLVD2102供电电压是2.5V+/-5%,不推荐直接把3.3V电平输入加到其输入端。建议解决方法如下:
1)电阻分压,在终端加分压电阻到2.5V的最大电平
2)采用CDCLVP2102实现3.3V直接输入
如果你的输出也是LVCMOS电平的话,可以考虑CDCLVC1102,CDCLVC1104系列