This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS1246采样率和模拟信号输入频带的问题~~望高手不吝赐教

Other Parts Discussed in Thread: ADS1246

我想选用ADS1246进行AD转换,该型芯片的采样率为2K,我的模拟信号中感兴趣的频带约为20-700Hz,已经进行了信号调理,前端拥有模拟低通滤波处理。我的问题是:按照采样定理,采样率为2K,那么我的新号频率就不能高过1K,对于高过1K的信号,模数转换芯片会怎么处理?从另一个角度说,ADS1246的采样率会不会起到类似“1KHz低通滤波器”的效果?另外作为一款成熟的商业化芯片,超过采样率范围的信号是否会对采样率内的信号产生影响而造成失真?

  • ADS1246是过采样原理的ADC,和奈奎斯特型不同,其采样率可以理解为调制率,约为512k,远高于2k的数据输出速率,从混叠失真角度不用担心。

    ADS1246内部会有数字低通滤波器,2k数据输出时,截止频率在1.5kHz。