Other Parts Discussed in Thread: ADS1259, OPA735
在使用ADS1259时碰到个很奇怪的问题,ads1259的参考电压我接入的是正负2.5V,测量时发现正参考是2.5,负电源是-0.8,请各位大侠看看,电路如下
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
需要说明的是,如果您的参考电压需要是+/-2.5V,那么您的ADC就不能采用单极性电源,需要采用+/-2.5的双极性电源,注意datasheet上的规格:
Negative reference absolute input (VREFN to DGND): AVSS –100mV ~ VREFP – 0.5 V
按照您的接法AVSS=0, 那么VREFN的最低电压将是-0.1V, 不可以是-2.5V,这样可能导致芯片烧掉(通常内部都是有保护二极管),这个也是你VREFN电压异常的原因。