This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

pcm4220采集的信号幅值变化较大的问题

Other Parts Discussed in Thread: PCM4220

你好!这是pcm4220的内部数字抽点滤波器幅频图像。

如图所示,我在采样频率为54khz 下采集2khz的信号,实质上2/54=0.037 此时位于通带范围内。同理当我的采样频率为51.2khz时采集2khz的信号,实质上2/51.2=0.039 此时任在通带范围内。依次类推采样频率为25.6khz时采集2khz信号,实质上2/25.6=0.078此时任在通带范围内。采样频率为20.48khz时采集2khz信号, 实质上2/20.48=0.097此时任在通带范围内。

从手册中截取的上图,可得知在通带范围内纹波在0.0015dB 这个范围非常的小,则振幅的幅值应该变化非常的微小。

但是如下数据表所示,在采集频率分别为54khz 、51.2khz、25.6khz和20.48khz下

采集2khz、 1vpp的信号 ,发现单峰幅值变化很大,幅度在几十mv。

采样频率(hz)

得到的信号单峰幅值(mv)

54k

992

51.2k

987

25.6k

952

20.48k

946

所以向你请教,造成这种现象的原因可能有哪些,对你提供的帮助感到万分感激!