This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298EVM 测量输入阻抗时出现很大干扰

Other Parts Discussed in Thread: ADS1298

使用检测中心的测量仪器EGC进行输入阻抗测试,输入10Hz,5mV的正弦波信号,记录一段时间,然后加入620K电阻,再记录一段时间;波形如下:

图1 未加入620K电阻

图2 加入620K电阻

图3 连续采集的波形对比

我自己使用ADS1298设计的硬件(电池供电)进行测试也是这种情况,但是使用我公司的其他ECG仪器测试得到的波形却没有干扰;

不知道如何改进,求指点

下面是输入阻抗测量的标准:Z是620K电阻与4.7nF电容并联的阻抗