This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS129X AFE4400 电源问题

ADS1x9xECG-FE评估板中电源回路的问题

我观察到本方案框图如下

但它只使用了两个LDO型的稳压器件把A;D两路的电压稳定至3&3.3;而通常锂电池的工作区间为2.5-4.2,这样一来,在2.5-3.5这个区域按此架构不能实现正常工作

但使用升压器件,均会带入电源回路一较大噪声,请问:

1.是否有满足ADS129X系列的升压器件或多个器件配合可达成近似功能,用于达成优化电池续航时间的目的,同时尽可能的保证AFE的采集精度

2.ADS129X系列对模拟电源的噪声要求是否有确定的数据可供参考?

3.我的设备还在新设计阶段,有ADS129X测量ECG和AFE44XX测量SPO2的需求,电池供电,为了续航考虑使用升压器件把2.5-4.2的输入稳成3.5V(TPS63000)但实测其噪声大约最大在100mV量级,是否有

是否对之后的采集会有影响?

  • 问题1:升压电路的输出纹波不单取决于控制器件本身,更大程度上也和外围功率器件有关,例如电感、电容等。所以,很难说哪个控制器行,哪个控制器不行。实际上,由于ADS129X内部数字滤波器的缘故,它对于电源纹波噪声并不是非常敏感,即使噪声比较大的升压DC/DC,只需在后端加上适当的处理,例如比较重的滤波,噪声性能比较好的LDO等,基本上都可以满足要求。

    问题2:不同频率的电源噪声对ADS129X的影响是不同的,同时,电源噪声的频率成分很复杂,因此,很难给出一个确切的对于电源噪声的要求。

    问题3:100mV显然太大了,一定会对采样造成影响。

    John