您好!
之前看LDC1000技术文档时,看到有一些应用,例如下面两个应用模式。想问一下,图中显示是包含了两个线圈甚至三个线圈,但是只是有一个电容和LDC1000,这个实际表示是需要两个LDC1000分别与LC sensor构成检测电路呢,还是如图显示的一个LDC1000加上LC sensor,只是可以同时接两个线圈甚至三个线圈?如果是后者,应该怎么实现?是否有资料可以参考?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢。
我知道这是属于两个不同的例子,我的意思是针对其中一个例子来说吧,好比第一个“Differential design removes z-axis dependence”,说明中用了一个LDC1000,一个电容,外部接了两个线圈。其实,我就想知道这个是运用了两个LDC1000芯片分别与一套LC sensor组成的,还是说只用了一个LDC1000芯片与一个电容,外部接两个线圈组成的。如果第二种情况,那具体实现形式是什么?