This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8686S: ADS8686S芯片性能指标是否会随着时间推移老化

Part Number: ADS8686S
Other Parts Discussed in Thread: ADS8688

2021年初生产的产品,当年测试时性能指标均满足要求。2023年再次测试时发现性能指标下降。

  • 您好,测试的哪些性能指标下降了?

    是不是储存条件影响的,受潮了吗?ADS8686S的潮湿敏感度是MSL3.

  • 您好,我们测试时ADC转换精度下降了一倍。还有两个问题,1、如果模拟量输入端超过±15V的脉冲信号,对ADS8686有影响吗?2、设备上电时出现AD输出全部为0后,程序中有监测BUSY位状态变化的看门狗程序,如超时未响应则将RST引脚下拉5ms,但是程序依旧未响应;直到重新上电才恢复。

  • 您好,关于您的问题,

    我们测试时ADC转换精度下降了一倍

    2021年购买,23年测试性能,发现转换精度下降了一倍是吗?

    1、如果模拟量输入端超过±15V的脉冲信号,对ADS8686有影响吗

    有影响,事实上,ADS8686S在使用时,5V供电,最大输入允许的电压范围为+-10V。 +-15V指的是 Absolute Maximum Ratings,引脚最大能承受的压力,并非功能性测试需要参考的参数,我们在使用芯片包括其他芯片时,需要参考的Recommended Operating Conditions。

    如果超过+-15V的电压,首先芯片性能不能保证,甚至能造成芯片永久性损坏。

    2、设备上电时出现AD输出全部为0后,程序中有监测BUSY位状态变化的看门狗程序,如超时未响应则将RST引脚下拉5ms,但是程序依旧未响应;直到重新上电才恢复。

    和您确认下,您上面提到的精度降低一倍,以及遇到的这个问题,是否都给了超过+-10V或者+-15V的电压范围,如果这样的话,我的建议是更换芯片,可能暂时通过重启能恢复,但是过压带来的过应力对芯片的损伤,将影响芯片部分电气性能。

  • 您好!

          谢谢您的答疑。

          我们使用ADS8686S时,偶尔上电后发现ADS8686S输出转换数据全部为0,读取自检数据也非0xAAAA和0x5555。通过论坛发现有使用ADS8688的用户遇到ADS8686因上电时序问题出现ADS8688宕机,即使是通过RST复位引脚重新复位都不能正常工作,直到重新上电为止。请问,ADS8686有相同的现象吗?即会出现宕机的情况。

          期待您的答复Pray

  • 通过论坛发现有使用ADS8688的用户遇到ADS8686因上电时序问题出现ADS8688宕机,即使是通过RST复位引脚重新复位都不能正常工作,直到重新上电为止。请问,ADS8686有相同的现象吗?即会出现宕机的情况。

    您好,合理的上电时序是保证芯片能正常工作以及寄存器能正常读写的基础,所以对于有上电时序要求的芯片,我们建议是严格按照芯片datasheet中的上电时序,否则可能会出现一些意想不到的结果。就像您说的ADS8688不合理的上电时序导致宕机,应该也不是绝对现象。那对于8686我不能保证是否也会出现宕机,但是仍建议按照datasheet中的上电时序,电气参数去使用,以便达到最优性能。