This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1212与ADS1230

Other Parts Discussed in Thread: ADS1230

TI工程师:

        您好!最近在做一个静态应变调理电路,要求分辨率为1个微应变,温漂为±2微应变。我想选用ADS1212或ADS1230,但前者价格较贵,考虑到我的采样频率仅为1Hz,所以我倾向使用ADS1230。但是比较这两者的系统性能后,我发现一些性能我无法辨别好坏,如这两者的噪声水平和温漂性能。所以无从决定选择哪一个芯片,还请各位赐教!谢谢

  • 看指标,你的要求还是蛮高的。建议用高指标芯片。

  • 从温漂性能上看ADS1212和ADS1230的性能接近,但是噪声性能无法比较。我想ADS1212的价格这个高可能是跟它的内部结构较为复杂有关,从共模抑制,温漂,电源噪声抑制这些性能上分析,两者相近,只是数据页中关于噪声的部分,两者的表述不一致,所以无从分析。还请各位帮帮忙,看看ADS1230能否取代ADS1212(这个芯片价格太贵了,呵呵),谢谢

  • 这两个IC差异很大,一个是22位;另一个是20位。性能基本要差一个量级。建议先核查一下识别精度是否够。

  • 然后;在冗余一倍分辨率的条件下;以就低不就高的原则,选取。如果没办法确认,还是选高指标的为妙。

    抱歉,因不知你的应变片设置情况,很难给出足够经济且够用的选择。其实,噪音问题是个老大难问题,它不光来自IC,不适当的连接及PCB布局;不合适的外围选取等都是致命的。正因如此;一般建议设定一倍的噪音、温漂冗余度。

  • 感谢您的帮助!我的应变片采用半桥形式,2个内置精密电阻加2个外接应变片,之前用分立器件搭建了调理电路:恒流源供电+AD8428(2000倍固定增益仪用运放)+4阶有源低通滤波。测试发现温漂性能比较糟糕。测试后发现问题是放大倍数过大后,即使是很小的增益温漂也会导致比较到的输出温漂,所以才想到用较小的增益外加较高分辨率的AD来做。由于时间和经费的限制,现在找到的这两款芯片,想比较后再做决定。您提到ADS1212比ADS1230的性能要好很多,不知是指那些方面,还请赐教,谢谢!