This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教:LMP90100的基准应怎样连接合适?



   

    在DATASHEET关于VREF介绍,这段话(For optimal performance, VREF should be the same as VA and sourced with a clean source that is bypassed with a ceramic capacitor value of 0.1 μF and a tantalum capacitor of 10 μF. ) 是不是可以理解为VREF可以直接从VA引脚一过来,中间加一个0.1 μF陶瓷电容和一个10 μF钽电容就可以?

    另:LMP90xxx also allows ratiometric connection for noise immunity reasons. A ratiometric connection is when the ADC’s VREFP and VREFN are used to excite the input device’s (i.e. a bridge sensor) voltage references. This type of connection severely attenuates any VREF ripple seen the ADC output, and is thus strongly recommended.  这句话怎么理解?