This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于AD转换器ADS805E的若干问题



1.使用0-5V伏量程时需要将vref和INn连接一起,Sel接地,此时INn端的共模电压2.5v是由vref端提供吗?还是需要在REFT和REFB间连接两个电阻分压后接到Vref?

2.手册上说明在2V量程时,REFT为3V,REFB为2V;但是并没有说明在5V量程时的电压,实测分别为3.76和1.26是否正确?如REFT和REFB电压有误差,请问和什么有关系?

3.ADS805E采用交流耦合连接的方法,信号输入端加隔值电容。用万用表实测当隔直电容前端(隔直电容前端连接AD)电压为零时,获得ADS805E的输出数字量不断变化,变化范围为20mv,可能是什么原因导致的(输入时钟1MHz)??

4.从信号测量准确度来看,使用2V量程和5V伏量程对于ADS805E哪个更有优势?

5.采用5v量程时,如信号超出5v,会不会烧坏ADS805E,OVER一直为高吗?(有人测试OVER变低了,为什么);若采用2V量程,如电压大于2v峰峰值,低于5v,是否对ADS805E有损害,OVER一直为高吗?

6.两个相同的ADS805E在同一块印制板,供电均为4.97v,选用5V量程,经测量其中一个REFT为3.76V,另外一个REFT为3.74V,为什么?可能什么原因会导致参考电压变化?

  • 在线等TI牛人回复

  • 第3条应为:

    3.ADS805E采用交流耦合连接的方法,信号输入端加隔值电容。用万用表实测当隔直电容前端(隔直电容后端连接AD)电压为零时,获得ADS805E的输出数字量不断变化,变化范围为20mv,可能是什么原因导致的(输入时钟1MHz)??

  • 1. 如果是内部参考,参照figure7,共模是由VREF提供的。

    2. 参照图6,产生共模电压,电压值为1.26+(3.76-1.26)/2=2.51。由于该电压只是提供共模电压,存在一定误差不会给电路带来太大影响。

    3.建议在电容和AD输入前加入一个小于100欧的电阻,参周数据手册的说明。你这里前面加运放了吗?如果有运放,不加电阻可能会导致不稳定,增加了噪声和失真。

    4.数据手册并没有给出两者的performance区别,参考电压对SNR没有什么影响。可以根据实际信号大小进行选择。

    5.maxmum rating中,输入范围最大为+VS+0.3v,如果是5v电源,输入信号不应超过5.3v。输入信号低于REFB或者高于REFT,OVER会变高

    6.器件之间会有一定差异。

  • 关于第3条的疑问:采用5v量程的时候,运放输出端首先连接一个RC低通滤波器(正常输入信号频率低于5KHz,连接的电阻为22欧姆,电容为100nf),然后再通过一个1uf的隔直电容和ADS805E的IN端相连,vref提供+2.5v共模电压给INn,IN端共模电压由两个2K的千分之一精度电阻分压(分别连接REFT和REFB),这种情况下,用万用表实测隔直电容前端(隔直电容后端连接ADS805E)电压为0,但是ADS805E获得的实测电压超过20mv了,这种连接方法已经加了电阻了,为什么还有那么大误差呢?

  • 如果每次测量的结果都是20mv左右,则怀疑是offset error。datesheet给出的zero-scale error为0.3%FS,则为15mv。