This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教ADC124S101这种没有参考基准电源的AD转换器的电源使用

Other Parts Discussed in Thread: LM4040, ADC124S101, LP2950

最近我要使用ADC124S101这个AD转换器,看其手册,该IC是没有内外参考基准电源的,只有一个VA管脚作为电源输入的。那么这个转换器是不是也以这个VA作为其AD转换时的基准参考?这个VA电源的精度是不是直接影响AD转换的结果?看手册中参考电路,是用LP2950的输出来给VA供电的,而LP2950的正常精度是1.4%(温度变化时达到2%),这样的电路来进行AD转换,似乎误差很大吧?用LM4040来供电应该更好吧?

另外发现有些DA转换器也是没有Ref脚,只有VA的,其供电也是与上面的AD类同吧?

  • 由于ADC124S101是一颗12位的ADC。因此在datasheet上推荐了用低噪声LDO来供电。你所提到的用基准源供电也是可以的,但LM4040不合适。它构成的电路驱动电流偏小。ADC124S101的最大工作电流是3mA。如果你想保证精度下,又不太在意成本的话。推荐使用REF5030A系列基准源。它的输出电流驱动能力是10mA。可以满足这个ADC的供电需要。

  • 你所说的这样的DA情况也是类似的,这路情况一般精度较低的数据转化器中才会出现基准与电源共用引脚的情况。

  • 感谢回复。

    但似乎你看错了文档吧,我看LM4040的手册,是这么描述的:Wide Operating Current Range…45μA Typ to 15mA ,其输出电流可以达到15mA啊。这个输出比REF5030A系列的10mA还要大哦,不过精度比不上REF5030

    麻烦再帮我确认一下哈。

  • 我这个系统的精度要求不算高,所以选用了12bit的AD和DA,不过用LP2950感觉也太粗糙了一点,所以想选个输出电流大一些的电压基准来做它们的电源。