最近用ADS1147测量一个正负传感器信号,数字电源为5V,模拟电源用的是+-2.5V,基准用片内的。在信号为正时,测量0~2V的信号,输出数据相应为0~65535,在负信号测量时,在-1V~0时为65535~32768,但是在-2V~(-1V)时,输出数值为0~32767,看说明这个输出不是二进制补码吗,在-2V~0应该是8000~FFFF,0~2V时为0~7FFF。以前只测量正信号,模拟电源也是0-5V,输出一直是0~65535,也成线性没在意。现在这个是我程序有问题吗?还是电源配置的不对?设置是内部2V参考一直打开。谢谢!附件是1147配置图