在同样的信号输入下,0.385V,PGA=1时,读出值是1576963,很正常,可是PGA=4时,读出值是2523145,跟前面值不是4倍的关糸,后来FULL GAIN REG写进2.5*0x40000,输出值才是跟PGA=1时,有四倍的关糸,为何满度增益校正寄存器写进这么大的值呢,跟原来的感觉相差很大,我以为输到ADC的值为0.385*4,不要校正即可得到4倍的值,6307839左右。请FAE给解答。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
即然是自动装载,PGA=4,跟PGA=1的转换结果应是4倍的关糸啊.
你好,ADS1247有输入电压要满足共模输入范围,请确认是否输入电压满足共模输入范围的要求
yijun zhen 说:确认是共模电压不在合适范围,现在调整了硬件,结果可以了。
请问楼主是调整了哪些方面的硬件呢?我也来学习学习、
这个项目是用在热电偶测温上的,调正了共模电压,差分电压二端提升了,
你好,我现在用ads247 AIN1=GND,AIN2为模拟信号输入,当AIN2输入为0,也就是接地时采集数据位1A7000,当输入为1.6V时为7FFFFF,PGA=1,可我要求的范围是0---2.5V,该怎么调增寄存器,我试了好多次值都不行,当为0时采集的数据比1A7000还大,我希望的是当为0时采集为0000000, 2.5V时采集为7FFFFF,该如何调整