This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP7002引脚输入问题

Other Parts Discussed in Thread: TVP7002

您好!请问TVP7002的COAST引脚,如果想使用外部输入,应该输入什么样的信号?TVP7002的EXT_CLK引脚,如果使用外部时钟作为像素时钟和ADC采样时钟,内部寄存器需要做哪些配置,外部电路需要做哪些修改?

  • 我以前使用的TVP7002,你可以参考下。

    在配置TVP7002之前,需要通过CPLD选通TVP7002的I2C通道并使能芯片,然后通过I2C配置TVP7002的各个I2C寄存器使其正常工作。在配置TVP7002为某种工作模式之前,需要先将TVP7002进行软件复位然后才开始配置。

    TVP7002的寄存器配置如下所示。

         /* TVP7002 - 1080i@60Hz - 33.75 Khz - 74.25Mhz - 20bit 4:2:2 - Embedded Syncs */

        errors |= tvp7002_rset( 0x01, 0x89 );   // PLL DIVMSB   2200

        errors |= tvp7002_rset( 0x02, 0x80 );   // PLL DIVLSB

        errors |= tvp7002_rset( 0x03, 0x98 );   // PLL CONTROL

        errors |= tvp7002_rset( 0x04, 0x80 );   // PHASE SEL(5) CKDI CKDI DIV2

     

        errors |= tvp7002_rset( 0x05, 0x32 );   // CLAMP START

        errors |= tvp7002_rset( 0x06, 0x20 );   // CLAMP WIDTH

        errors |= tvp7002_rset( 0x07, 0x60 );   // HSYNC OUTPUT WIDTH - 96

        //errors |= tvp7002_rset( 0x0e, 0x20 );   // SYNC CONTROL    HSout+

        errors |= tvp7002_rset( 0x0e, 0x1b );

     

        errors |= tvp7002_rset( 0x0f, 0x2e );   // PLL and CLAMP CONTROL

        errors |= tvp7002_rset( 0x10, 0x5d );   // SOG Threshold-(YPbPr Clamp)

        errors |= tvp7002_rset( 0x11, 0x47 );   // SYNC SEPERATOR THRESHOLD

        //errors |= tvp7002_rset( 0x12, 0x00 );   // PRE_COAST

        errors |= tvp7002_rset( 0x12, 0x01 );    // PRE_COAST

        errors |= tvp7002_rset( 0x13, 0x00 );   // POST_COAST

        errors |= tvp7002_rset( 0x15, 0x47 );   // Output Formatter, 64-960, embedded syncs

        errors |= tvp7002_rset( 0x16, 0x01 );   // MISC Control

        errors |= tvp7002_rset( 0x17, 0x00 );   // Outputs enabled

        errors |= tvp7002_rset( 0x18, 0x01 );   // T-SW disabled, blank off, CSC disabled, FID, SOG, CLK polarity=invert

        errors |= tvp7002_rset( 0x19, 0x00 );   // INPUT MUX SELECT    CH1 selected (BNC )

        errors |= tvp7002_rset( 0x1a, 0x67 );   // SOG Filter(10Mhz) and CLP, INT REF CLK, INPUT MUX SELECT  HSYNC_B and VSYNC_B selected

     

        errors |= tvp7002_rset( 0x21, 0x08 );   // HSOUT START

        errors |= tvp7002_rset( 0x22, 0x00 );   // Macrovision support

        errors |= tvp7002_rset( 0x26, 0x80 );   // ALC Enable

        errors |= tvp7002_rset( 0x28, 0x53 );   // AL FILTER Control

        errors |= tvp7002_rset( 0x2a, 0x07 );   // Enable FINE CLAMP CONTROL

        errors |= tvp7002_rset( 0x2b, 0x00 );   // POWER CONTROL-SOG ON

        errors |= tvp7002_rset( 0x2c, 0x50 );   // ADC Setup

        errors |= tvp7002_rset( 0x2d, 0x00 );   // Coarse Clamp OFF

        errors |= tvp7002_rset( 0x2e, 0x80 );   // SOG Clamp ON

        errors |= tvp7002_rset( 0x31, 0x5a );   // ALC PLACEMENT

     

        errors |= tvp7002_rset( 0x34, 0x02 );   // Macrovision Stripper Width

             //errors |= tvp7002_rset( 0x3e, 0x04 );

        errors |= tvp7002_rset( 0x3f, 0x01 );   // Input B/W

     

        errors |= tvp7002_rset( 0x40, 0x06 );   // AVID Start  262 (236+26) 27-1 for SOG filter differnence

        errors |= tvp7002_rset( 0x41, 0x01 );   // AVID Start

        errors |= tvp7002_rset( 0x42, 0x8a );   // AVID Stop  2186 (AVID start + 1920 + 4)

        errors |= tvp7002_rset( 0x43, 0x08 );   // AVID Stop

     

        errors |= tvp7002_rset( 0x44, 0x02 );   // VBLK F0 Offset

        errors |= tvp7002_rset( 0x45, 0x02 );   // VBLK F1 Offse

        errors |= tvp7002_rset( 0x46, 0x16 );   // VBLK F0 Duration

        errors |= tvp7002_rset( 0x47, 0x17 );   // VBLK F1 Duration

    TVP7002的COAST引脚,如果想使用外部输入,应该输入高电平

    使用外部时钟作为像素时钟和ADC采样时钟,内部寄存器需要做哪些配置,外部电路需要做哪些修改?

    使用外部时钟作为像素时钟和ADC采样时钟,内部寄存器需要做哪些配置,外部电路需要做哪些修改?
    TVP7002的EXT_CLK引脚,如果使用外部时钟作为像素时钟和ADC采样时钟,时钟频率可以从0到27 MHz选择使用。内部寄存器需要做选择子地址为1AH。。
  • 如果想使用外部输入,COAST引脚输入矩形波信号。不用时候可以接地。

    如果使用外部时钟,需要把CLK SCL寄存器置1,采用外部时钟。外部电路只需在EXT_CLK管脚加入时钟信号即可。

     

  • 您好,感谢您的回复!请问您所说的矩形波信号是什么样的呢?比如占空比和频率。

  • 你好,我的外部时钟给27M,CLK SEL设置为1,输入信号为1080p60,但是输出的DATACLK也是27M,请问哪里还有需要注意的吗?