Other Parts Discussed in Thread: THS4521, ADS1278
你好,
你好,上图电路就是ads1278推荐的单端转差分驱动电路,现在的问题是上电测量VIN端有1.67V的电压,AINP和AINN之间的压差也是1.67V。片子VOCM管脚我加了一个2.5V的直流参考电平,这时候就导致如果在VIN端加交流信号会叠加一个1.67V的直流电平,而AINP和AINN所出来的差分信号不是以2.5V为基准的差分交流信号。
我想问一下,上图给出的ths4521单端转差分电路是正确的吗,好像和ths4521的datasheet里面的单端转差分原理图(如下图)不一致吧。
另外,想请教一下ads1278高速模式和高精度模式下所能得到的最高精度是多少。根据你们给的信噪比和精度之间换算的公式,高精度模式最高精度能达到18位,高速模式达到17位,是不是这样的。
谢谢各位大神给予帮助