This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CD4013电源的问题



        我想使用CD4013对振荡器产生的100KHz、+/-7.5V方波信号作二分频和四分频,因此选择了CD4013双D触发器。但是我使用万用板搭建电路试验时,发现该触发器使用+/-7.5VDC电源供电条件下不能正常工作;而我将VSS端接到GND时能够正常工作,但是只有正半波,不是我想要的结果。我在datasheet上看到,VDD相对于VSS的电压可以使-0.5~20V(最大绝对额定值),所以我认为这种芯片应该是可以使用正负电源对输入+/-7.5V方波信号分频的,可是为什么芯片不能工作呢?如果这种芯片不能正常工作,那么可以采用什么芯片对上述信号分频呢?以前使用CD4060、CD4007时都是+/-7.5VDC供电,一直没什么问题,但这次为什么就不好使呢?在下实在不解,跪求各路大神赐教!

  • 4013对输入信号陡度和幅值有一定要求。因此;即便是双极性波也要满足以负电源为参考的逻辑要求。

    所以,建议亲先用CD4050等缓冲;再用缓冲后的信号供给4013。

  • 您好,我今天又用了CD4027作分频试验,仍使用+/-7.5V电源供电,结果还是无法实现分频,CD4027输出是一个固定的7.5V。据我的试验结果,是不是说明CD4013、CD4027这类触发器不能使用正负电源供电呢?但是datasheet上说的电源指标-0.5~20V是相对于VSS的啊。而且CD4060这样的分频器,电源指标与CD4013相同,接+/-7.5V电源就是可以正常工作的~~

  • 4000系列是可以双电源工作的,但!特别是。。。参考地,必须以负电源作为信号参考地!!!!否则,无法工作。

  • 我总算明白为什么不能正常工作了~~确实是您说的那样,我把触发器的R/S端都接到了GND,而不是接到VSS,所以才无法工作。以后我对正负电源供电的芯片都以VSS作为参考地。谢谢啦!