LDC1000的VIO接口可以接5V电源吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个关键看你IO逻辑电平是多少?参见手册5,6页
VIO IO Supply Voltage VIO≤VDD 1.8 3.3 5.25 V
SYMBOL PARAMETER CONDITIONS/ MIN(3) TYP(4) MAX(3) UNITS COMMENTS
DIGITAL I/O CHARACTERISTICS
VIH Logic "1" Input Voltage 0.8×VIO V
VIL Logic "0" Input Voltage 0.2×VIO V
看下面,但是只有第一页是中文,后面是英文,哪儿看不明白可以提出来
http://www.ti.com.cn/cn/lit/ds/symlink/ldc1000.pdf
为什么我读出的数据固定不变?拔掉SDI的连接线再连接上,每次重复操作都会改变读出来的数据,但用金属靠近电感线圈,数据不变。