正在调DAC8571,按如图的连接做的小模块,采用模拟I2C的方式。不管发送的是多少,输出都有几到几十毫伏(应该是噪声)。读出的都是32767。还没找出是什么原因,希望有人帮忙看看错误出在哪里了。在此先谢过了。
模拟IIC的代码
//***************************IIC.c*********************************************
//产生IIC起始信号
void IIC_Start(void) { SDA_OUT();
IIC_SDA=1; IIC_SCL=1;
delay_us(4); IIC_SDA=0;//START:when CLK is high,DATA change form high to low delay_us(4); IIC_SCL=0; } //产生IIC终止信号
void IIC_Stop(void) { SDA_OUT();
IIC_SCL=0; IIC_SDA=0;//STOP:when CLK is high DATA change form low to high delay_us(4); IIC_SCL=1; IIC_SDA=1;/
delay_us(4); }
u8 IIC_Wait_Ack(void) { u8 ucErrTime=0; IIC_SDA=1;delay_us(1); IIC_SCL=1;delay_us(1); SDA_IN();
while(READ_SDA) { ucErrTime++; if(ucErrTime>250) { IIC_Stop(); return 1; } } IIC_SCL=0; return 0; }
void IIC_Ack(void) { IIC_SCL=0; SDA_OUT(); IIC_SDA=0; delay_us(2); IIC_SCL=1; delay_us(2); IIC_SCL=0; } void IIC_NAck(void) { IIC_SCL=0; SDA_OUT(); IIC_SDA=1; delay_us(2); IIC_SCL=1; delay_us(2); IIC_SCL=0; }
void IIC_Send_Byte(u8 txd) { u8 t; SDA_OUT(); IIC_SCL=0;
for(t=0;t<8;t++) { IIC_SDA=(txd&0x80)>>7; txd<<=1; delay_us(2);
IIC_SCL=1; delay_us(2); IIC_SCL=0; delay_us(2); } } u8 IIC_Read_Byte(unsigned char ack) { unsigned char i,receive=0; SDA_IN();
for(i=0;i<8;i++ ) { IIC_SCL=0; delay_us(2); IIC_SCL=1; receive<<=1; if(READ_SDA)receive++; delay_us(1); } if (!ack) IIC_NAck();
else IIC_Ack(); return receive; }
//************************************IIC end***************************************************
//***********************************DAC.c*****************************************
void DAC8571_Init(void) { IIC_Init(); } void DAC8571_Write(void) { IIC_Start(); IIC_Send_Byte(0x98); IIC_Wait_Ack(); IIC_Send_Byte(0x10); IIC_Wait_Ack(); IIC_Send_Byte(0xff); IIC_Wait_Ack(); IIC_Send_Byte(0xff); IIC_Wait_Ack(); IIC_Stop(); } unsigned int DAC8571_Read(void) { unsigned int temp1,temp2; IIC_Start(); IIC_Send_Byte(0x99); IIC_Wait_Ack(); temp1 = IIC_Read_Byte(1); // temp1 <<= 8; temp2 = IIC_Read_Byte(1); temp1 = temp1*256+temp2; IIC_Send_Byte(0x20); IIC_NAck(); IIC_Stop(); return temp1; }
//******************************DAC.c end********************************