Other Parts Discussed in Thread: DAC8571
正在调DAC8571,按如图的连接做的小模块,采用模拟I2C的方式。不管发送的是多少,输出都有几到几十毫伏(应该是噪声)。读出的都是32767。还没找出是什么原因,希望有人帮忙看看错误出在哪里了。在此先谢过了。
模拟IIC的代码
//***************************IIC.c*********************************************
//产生IIC起始信号
void IIC_Start(void)
{
SDA_OUT();
IIC_SDA=1; IIC_SCL=1;
delay_us(4); IIC_SDA=0;//START:when CLK is high,DATA change form high to low delay_us(4); IIC_SCL=0; } //产生IIC终止信号
void IIC_Stop(void)
{
SDA_OUT();
IIC_SCL=0; IIC_SDA=0;//STOP:when CLK is high DATA change form low to high delay_us(4); IIC_SCL=1; IIC_SDA=1;/
delay_us(4); }
u8 IIC_Wait_Ack(void)
{
u8 ucErrTime=0;
IIC_SDA=1;delay_us(1);
IIC_SCL=1;delay_us(1);
SDA_IN();
while(READ_SDA)
{
ucErrTime++;
if(ucErrTime>250)
{
IIC_Stop();
return 1;
}
}
IIC_SCL=0;
return 0;
}
void IIC_Ack(void)
{
IIC_SCL=0;
SDA_OUT();
IIC_SDA=0;
delay_us(2);
IIC_SCL=1;
delay_us(2);
IIC_SCL=0;
}
void IIC_NAck(void)
{
IIC_SCL=0;
SDA_OUT();
IIC_SDA=1;
delay_us(2);
IIC_SCL=1;
delay_us(2);
IIC_SCL=0;
}
void IIC_Send_Byte(u8 txd)
{
u8 t;
SDA_OUT();
IIC_SCL=0;
for(t=0;t<8;t++)
{
IIC_SDA=(txd&0x80)>>7;
txd<<=1;
delay_us(2);
IIC_SCL=1;
delay_us(2);
IIC_SCL=0;
delay_us(2);
}
}
u8 IIC_Read_Byte(unsigned char ack)
{
unsigned char i,receive=0;
SDA_IN();
for(i=0;i<8;i++ )
{
IIC_SCL=0;
delay_us(2);
IIC_SCL=1;
receive<<=1;
if(READ_SDA)receive++;
delay_us(1);
}
if (!ack)
IIC_NAck();
else
IIC_Ack();
return receive;
}
//************************************IIC end***************************************************
//***********************************DAC.c*****************************************
void DAC8571_Init(void)
{
IIC_Init();
}
void DAC8571_Write(void)
{
IIC_Start();
IIC_Send_Byte(0x98);
IIC_Wait_Ack();
IIC_Send_Byte(0x10);
IIC_Wait_Ack();
IIC_Send_Byte(0xff);
IIC_Wait_Ack();
IIC_Send_Byte(0xff);
IIC_Wait_Ack();
IIC_Stop();
}
unsigned int DAC8571_Read(void)
{
unsigned int temp1,temp2;
IIC_Start();
IIC_Send_Byte(0x99);
IIC_Wait_Ack();
temp1 = IIC_Read_Byte(1);
// temp1 <<= 8;
temp2 = IIC_Read_Byte(1);
temp1 = temp1*256+temp2;
IIC_Send_Byte(0x20);
IIC_NAck();
IIC_Stop();
return temp1;
}
//******************************DAC.c end********************************