Other Parts Discussed in Thread: ADS1278
ADS1278芯片上电发现温度慢慢上升,到最后很烫手 估计温度有七八十度了,其中我的测试板芯片底座的热焊盘连接在接地引脚并打了过孔,用DSP给了20M的clk信号给ADS1278.其中模式设置为MODE[1..0]00高速模式 格式为FORMAT[2..0]001设为SPI模式。各个供电引脚都正常AVDD=5V,DVDD=1.8V,IOVDD=3.3V,Vcom输出2.5V也正常。用示波器观察发现DRDY一直处于低电平。用热风枪吹下来,我测量芯片各通道对地的阻抗 大概有7M,不知道是否正常。其中焊接芯片的烙铁温度为370度,热风枪吹大概也有400度。看手册上写焊接温度为150度,但150度根本无法焊接啊,不知道是不是焊接有没有可能焊坏了芯片。