您好,我最近在用ADS1256,想要你给他来采集一个单端电压信号。折个电压信号在0~5V范围内。
我仔细阅读了ADS1256的数据手册,发现他确实可以连接单端信号,只不过是伪差分模式的,即:我的AINCOM如果接2.5V,PGA选择1,就可以接这个0~5V单端信号。但是,我的传感器是有两个信号线,一个是信号正,一个是信号GND。那么,我想请问,我这个信号该如何连接到ADFS1256的引脚上呢?难道是?我的信号正,连接到ADS1256的某一个IN引脚上?而我的信号GND连接到那个有2.5V的AINCOM引脚上?
还有,我看技术手册上说,ADS1256引脚的AINCOM建议接2.5V的电压,即:不要接GND,技术手册上到:
When using ADS1255/6 for single-ended measurements,
it is important to note that common input AINCOM does not
need to be tied to ground. For example, AINCOM can be
tied to a midpoint reference such as +2.5V or even AVDD.
那么,我想请问,作为单端信号,我该怎么处理这个AINCOM引脚呢?!