This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1271问题

Other Parts Discussed in Thread: ADS1271

我在AVDD为5V,DVDD为3.3V,工作频率为25M,SCLK为6.25M,Frame_Sync模式的情况下使用ADS1271,模拟输入端为零时输出数据的高几位(大概是D23到D12)为什么总是高电平?理论上只有最高位才有可能是高电平的么。

  • 你的ADS1271是跑在什么工作模式下?

    模拟输入为零的时候,受偏置电压等影响,输出结果可能略小于0,那么这个时候的数据输出就是很高位很多为1。具体请参考数据手册Table 9. Ideal Output Code versus Input Signal