我的ADS1256用来测量两路模拟信号,分别为AIN0和AIN1,按照Datesheet中Page21中的Figure19中的时序写的程序,但我发现当采样频率为2.5SPS到1KSPS之间时只能读出一个通道的数据,而当采样频率大于1KSPS时可以正常读出两个通道的数据,这是怎么回事呢?各位TI专家有没有遇到过这种问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的ADS1256用来测量两路模拟信号,分别为AIN0和AIN1,按照Datesheet中Page21中的Figure19中的时序写的程序,但我发现当采样频率为2.5SPS到1KSPS之间时只能读出一个通道的数据,而当采样频率大于1KSPS时可以正常读出两个通道的数据,这是怎么回事呢?各位TI专家有没有遇到过这种问题?
在高采样率和低采样率的SCLK都是625kpbs,两个通道分别输入1V和0.5V的电压信号,在多片ADS1256上都是这样的。
按照Figure19中所示,在写MUX SYNC WEAKUP 之后DRDY会变高,这时会有个t18的SETTING TIME,然后DRDY变低,然后接着写下一个通道,如果在程序中根据DRDY的高低变换来写这个循环的话 就会只读出一个通道的数值。
后来我在两个通道切换之间加了延迟就能分别读出两个通道的值了,这个延迟就是Table13.里面给的SETTING TIME(t18),也就是在写MUX,SYNC,WEAKUP,RDATA,之后加了t18的延迟,等待DRDY变低之后,再去写另外一个MUX,SYNC,WEAKUP,RDATA,然后再延迟t18,如此循环,才能正常读出两个通道的数值。
恭喜能正常读出数据,也感谢分享!
我有个疑问,按照图19所示的意思,DRDY 从在高电平的时间应该大于t18的. 请问你在延迟t18以后,DRDY的状态是高电平还是低电平的?
能否用示波器测试一下DRDY的高电平持续时间有多长?谢谢!