This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教ADS7830抗ESD干扰方法

Other Parts Discussed in Thread: ADS7830, ADS8688

我在用ADS7830做一个按键检测,在做3KV ESD测试时,ESD信号打到外壳的地时,ADS7830会锁死。当ESD信号撤销后,改变ADC的输入信号,输出都是干扰前的数据。以下是我做的一些测试:

1. 在输入端对地我加了小电容(即C110,C111,C112,C113,C123,C128),没有效果。

2. 在VDD和地之间靠近ADS7830处加了一个0.1uF 的电容,也没有效果。

3. 在Vref对地和VDD对地间分别加了5V TVS管,也没有效果。

请问还有什么办法能改善抗ESD干扰?以下是原理图供参考。--谢谢。