我使用6片ADS1271组成菊花链,使用FPGA SPI模式,最后一片DIN接地,第一片的DOUT作为数据输出,MODE、FORMAT接低,SYNC/PDWN接高电平,fpga通过第一片的DRDY判断数据是否开始转换,其他芯片DRDY不接。现在上电后虽然6片都有数据输出,但是我把第一片差分负端接地,正端接一固定电压(0-2.5v之间)时,第一路输出中间偶尔会出现一个大数,能看出完全不是正常数据。用示波器测量CLK为25M左右,但是第一片DRDY周期大概是50K左右。
请问1,这个DRDY是第一片的数据转换完就产生低电平还是6片都转换完产生一次?如果是6片数据都转换完产生一次,那频率怎么才50K左右,相当于一片的转换速度?如果是一片转换完产生一次,那后面5片是否转换完我怎么检测?
2,多片菊花链链接是不是必须上电同步才行?不同步可能会出现数据突然跳出大数的情况?