Other Parts Discussed in Thread: DAC8734
大家好,我在使用DAC8734的时候,了解到上电时序是先5V和3.3V,然后是15V和-15V,不使用继电器,不使用外部开关,请问怎样能做到+-15v的延时输出?看到DAC8734的EVM板子直接从外部接入几个电源,也没看到有上电的先后顺序,我们的系统里可以直接接入+-15v电源,但是怎么实现延时呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DAC8734
大家好,我在使用DAC8734的时候,了解到上电时序是先5V和3.3V,然后是15V和-15V,不使用继电器,不使用外部开关,请问怎样能做到+-15v的延时输出?看到DAC8734的EVM板子直接从外部接入几个电源,也没看到有上电的先后顺序,我们的系统里可以直接接入+-15v电源,但是怎么实现延时呢?
这个实际上您的如果您需要做供电电压的时序,您可以通过控制电源芯片的使能脚来做到,EN脚增加一个电容作延时,如果供电电源芯片没有使能脚EN, 就需要外部增加MOS控制信号的关断而达到控制时序的目的。
试一试能不能用5V控制3.3V的使能管脚?用3.3V控制15V的使能管脚