This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在前面“关于ADS1245的问题”这一帖子中Mr Martin推荐了用ADS1259等来对交流输电线电流的采样值进行转换,并写到:测交流输电线电流一般测个15次谐波就足够了!15*50=750Hz。
请问如果我在采集卡(或传感器)与AD芯片之间加上一个抗混叠滤波环节,那么是不是750Hz就是我在进行滤波器设计时所应考虑的最大分析频率,或者按照某些文献的说法可将截止频率定为最大分析频率即750Hz,不知道以上说法对不对?
另外,我是将截止频率设定为了320Hz左右,采样率为ADS1259(我用的ADS1259)的3.6Khz,是否合适呢?
谢谢了。
你好,那如果我按320Hz设置截止频率的话,那么是否可以理解为我测了320/50约为7次谐波,我这种理解对吗?测7次谐波的频率宽度和测15次谐波的频率宽度在输电线电流采集及AD转换(即此类应用)中有什么区别呢,如何理解这个频率宽度呢?这块我查找了一些资料还是没有搞明白,望指教。
谢谢了。
你好,
如果你用320Hz,7次谐波(350Hz)已经在带宽之外,会被抑制;你说的频率宽度应该就是指采样率吧,根据采样定理,采样频率必须是信号频率的两倍以上,所以测7次谐波(350Hz)采样率至少是700sps, 测15次谐波(750Hz)采样率至少是1.5ksps
您好,首先感谢您的回复。
然后,我想请教的是测15次谐波和测7次(或其它次)谐波是如何确定的,就是我应该测15次谐波,还是应该测7次(或其它次)谐波,这个次数的确定的依据是什么?
按照我现在电路的实际接法,截止频率只能为320Hz,我现在担心的是按照我320Hz截止频率的设定,测的谐波数只能是低于7次(即6*50=300Hz),那么这样的话能不能实现对输电线电流的有效采集及后续转处理呢,是不是测的谐波数太少了,这个有关系吗?