This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS1259的校准问题

Other Parts Discussed in Thread: ADS1259

我想请教一下ADS1259的OFC和FSC寄存器是怎么设置的呢,也就是怎样确定校准值呢,有什么对照标准吗?如果是芯片自校准的话,是不是取默认值就可以了,另外,全量程校准的时候是不是需要准确的全量程值呢?

  • ADS1259的校准需要外接输入。

    如果是芯片自校准的话,需要零输入和满量程输入两种信号。芯片自校准下的满量程校准是需要准确的满量程。

    具体请参考数据手册27页CALIBRATION章节的介绍

  • 请问你是用ADS1259做什么应用呢?需要同时做系统校零和满量程校准吗?会用到多少个输入通道?

  • 谢谢Martin。

    我是用ADS1259来做采集到电流值的AD转换的,只有一个输入通道,在AD芯片前面加了一个放大电路和抗混叠滤波电路。说实话,我是第一次做这方面应用,基础较差,现在是不知道需不需要进行校准,看了数据手册之后也不知道OFC、FSC寄存器设置的依据是什么。

  • 另外,我看数据手册第27页讲到进行calibration,首先“set the gate control mode”,而我的系统设计中CONFIG2寄存器设置的是"pulse control mode",这种情况下还能校准吗,是不是要对该寄存器重新初始化一次?