手册上说,vref为2.4v的时候,测试信号为1mv,算出来应该是X"DA7",但是实际测出来是方波,可是幅值为x"5000"?
这是为什么啊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个需要看到您的寄存器配置, 您是否是参考的datasheet (www.ti.com.cn/.../ads1298.pdf )第87页 Activate a (1mV*V ref /2.4) Square-Wave Test Signal?
按照这个参考, PGA=6, 测试信号1mV Vref=2.4V
1mV=2.4/(PGA*2^23) * Dout
Dout= 1mV* PGA*2^23/2.4 =5*2^12
即输出0x 5000.
计算如上, PGA=6, 2^10记做1000,可以得到Dout= 1mV* PGA*2^23/2.4 =5*2^12.