问题1、
计划使用1298做心电工作站,设计指标是0.05-150HZ
ADS1298的实际最大频带宽度为多少呢?看datasheet上说是开启EMI滤波网络后fc=3MHZ,也就是BW<3MHZ了?最后做好的东西使用不同频率、1mV的正弦波激励测试频带宽度,按照-3dB衰减算出来实际频带只有0.05-75HZ,其中0.05的高通滤波使用FIR数字滤波实现。请问为什么测出的上限频率这么窄呢?是寄存器配置问题吗?
问题2、
ADS1298按照24bit标准,最大增益只有12(Gain),取ECG信号最大5mV计算,为5*12=60mV,同时内部参考Vref取4V,(60/4000)*2^24=251658,按此数字量来说使用18bit的ADC也足矣,也就相当于损失了6bit精度的数据?对吗?