圆圈1中的320是什么意思?
配置寄存器数据写入和320 DCLK时钟脉冲后的回读数据结构是什么?
根据注和表9,16位配置寄存器数据,4位修订ID, 300位校验模式,怎么可能有1024 TOTAL READBACK BITS, format = 0 ?
4位的版本号是什么,怎么设置?
谢谢你的帮助!



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
“配置寄存器的可选回读在写入序列之后立即可用。”
NOTE显示“此输出序列对每个DDC264块重复两次”,
图30显示“在16位模式下(format = 0),在配置寄存器读写操作之前只读取256 0s”,
因此,我可以获得16位配置数据,然后是4位修订ID和236位检查模式两次 一共256*2 = 512位,在Configuration Register Operations期间写寄存器之后马上,在FORMAT = 0前提下,对吗?
在Normal Operation中我可以得到1024位,对吧?
但是4位修正是什么呢?
谢谢你的回复
您好,
320是指320个0 bits
回读数据结构:

怎么可能有1024 TOTAL READBACK BITS, format = 0 ?
图30 写的可能不清楚,这个320 0s是指在format =1时,在format = 0时,这里应该是256 个0
这样在format = 0时 总的位数是256+16+4+check pattern,
check pattern看table9是180个0+56bit (30F066012480F6h为56bits),这样是236bits
256+16+4+check pattern=276+236=512bits 乘以2是1024bits