Hi,想请教下DAC7718的供电可以为15V么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,DAC7718的AVDD电压范围为4.5V~18V,负压AVSS的电压范围为-18V~-4.5V范围,所以要同时满足AVDD和AVSS的电压范围才可以。
您指的15V,应该是AVDD=15V, AVSS=GND是吗?那这是不允许的,AVSS应该接的是-18V~-4.5V范围内的负压。
抱歉,我的描述可能不是很清楚。
我的意思是AVDD给15V的电压,AVSS给-15V的电压,在这个供电条件下DAC输出的电压范围还是-15V到15V之间么?
您好,模拟输出的幅值Vout计算可以参考公式1和2(分别再sce=0和sce=1的前提下)
最大输出幅值为AVDD-0.5V,最小输出为AVSS+0.5V。如果需要输出+-15V范围的话,最大输出+-14.5V,为了保证其输出不饱和的话,如果要达到+-15V输出的话,建议使用+-16.5V供电。