Other Parts Discussed in Thread: ADS1191
现在使用ADS1191搭建一个只使用两个电极的设备采集心电信号,根据ADS1191的数据手册以及ADS1X9X的用户手册,我采用IN2N和IN2P作为输入电极,不用的IN1N和IN1P就连在VDD上。RLD电路外接了反馈网络。
想请问:(1)这样的硬件连接能否正常工作?由于已经投板回来焊接好了,万一改动的话比较麻烦了。。。
(2)如果可以使用的话,RLD的三个引脚OUT,INV,IN应该怎么和内部信号相连,以及关于寄存器RLD_SENS的设置?
(3)我仔细看过手册中寄存器的设置,想知道如何实现RLD的提供共模电压以及抑制噪声的作用?
另外,ADS1191是单通道,那为什么有两个通道寄存器CH1SET 和CH2SET呢,这和硬件上的IN1,IN2又是什么关系呢?
已经卡住了很久了,迫切等待解答,多谢了!