如图的模拟域增强导联输出方式,下面是我用计算得出的aVL和通道5测量出的aVL,数值差异很大


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如下此视频中(https://www.ti.com/video/5423179122001)导联定义截图:

您是根据上述定义测量的吗?测量时 LL、RA和RL导联是否连接?您是使用的ECG模拟器产生的输入信号吗?
您是怎样计算得出的aVL?
因为您将LA(Left Arm)连接到 通道5的正极,因为我认为您的aVL定义是LA-(LL+RA)/2。需要您注意的是EVM板的通道5的正极如果按J1标注的信号连接,那么您应该将LA连接到标注V3的位置,而不是标注LA的位置。因为V3的位置才是通道5的正极。


而WCTA、WCTB、WCTC 放大器默认寄存器配置都是输入的ch1的正极,因此您这种配置并不能实现aVL信号的采集。
建议您先观看下面视频,了解ECG的测量方法: