This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298: 采用菊花链模式时,第二片板子不工作

Part Number: ADS1298

检查了寄存器配置没有问题,时钟的话,第一片1298使用内部时钟,并且时钟输出给第二片1298,但是我没有放在一个PCB板子上面,而是用杜邦线传输时钟和SPI通信的时钟和数据。现在就是第二片1298一旦接入系统,就会看到数据全部是00 00 00,没有开始采样转换,但是看示波器的CLK等波形都是对的,供电也正常,第一片1298可以工作,代码也没有问题,想问一下是时钟的问题吗?有没有人做过这种不在一个板子上的菊花链拓展呢?

  • 您好,

    您是按照下面Daisy-Chain 示意图连接的原理图吗?您是否可以缩短使用的杜邦线长度? 尽量缩短接线长度再测试结果怎样?

    如果缩短接线长度还不行,您可以附上原理图和寄存器配置吗?

x 出现错误。请重试或与管理员联系。