This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLA2528: TLA2528数据如何读出

Part Number: TLA2528


我在使用FPGA控制这款adc的时候遇到了以下几个问题

1.

我将adc配置成auto_sequence mode时,按照下列的配置顺序及配置值进行配置是否有误

(1)SEQUENCE_CFG :0X00

(2)PIN_CFG               :0X00

(3)AUTO_SEQ_CHSEL :0X1C

(4)SEQUENCE_CFG    :0X01

(5)DATA_CFG              :0X10

(6)SEQUENCR_CFG   :8'b11

(2)图中的Conversion Start Frame、Conversion Read Frame具体是怎么样的?

是按照Single Register Read的这种时序吗,如果是的话adc采样的数据应该从哪个寄存器读出,寄存器地址是0x0D吗?

还是说寄存器配置完成后,直接输入设备地址加上读标志位

2.我想将ad配置成high-speed mode,那么在配置成high-speed mode之前,我i2c所使用的时钟频率是否应该不超过Fast mode scl的最高频率1MHz