This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti
currently our ultrasound asic is development some function, tx/rx is analog zone then signal are differential pair. AFE5808 has 8-ch input and 8-ch LVDS outputs
my question is : i'm not sure LVDS (digital signal) connect to rx of ultrasound asic . because this asic don't accept clk of LVDS.
also i check the spec, input channels all connect to mixer than go to CW_OUT M/N then use switch to on off each channel.
so does I/Q_bus (CW_out) connect to RX of ultrasonic asic?
pls give me a suggestion!
thanks so much!!
您好,方便沟通我们可以直接使用中文讨论。
: i'm not sure LVDS (digital signal) connect to rx of ultrasound asic . because this asic don't accept clk of LVDS.
ASIC的差分输入支持什么电平输入?如果不支持LVDS,那么AFE5808的输出LVDS是不可以直接和RX接的,因为电平幅值和共模电压都不一样。
also i check the spec, input channels all connect to mixer than go to CW_OUT M/N then use switch to on off each channel.
so does I/Q_bus (CW_out) connect to RX of ultrasonic asic?
这里是什么意思?CW_out和ASIC的RX接在一起是吗?
首先CW_out 是summing amplifier的输出端,电压4Vpp,1.5V共模电压,是否能满足RX的电压要求?
那么关于CW_out是否和RX端连接,抱歉,ASIC的spec我不太熟悉,我认为它应该是和前端的TX连接的。而CW_out外部是要接LPF。或者悬空都是可以的。